FAQ Search

Want to add a CE3050B to an existing CDP panel?

The CE3050B breaker is obsolete.
The Replacement breaker is a Square D HDL36050 breaker with a HDCMH mounting kit. The breakers are rated at 14 KAIC.
The HDCMH will mount two H frame breakers.
An S37444 is included in the HDCMH to convert breaker from Lug-Lug to Lug-Pad. If a second breaker is being mounted on the HDCMH Hardware, order an additional S37444.
Hardware Kit requires both sides of panel and will only mount Powerpact H Breakers.


CTA-ID : 2053610
FA130352  |  14-Jan-2011  | Cross Reference
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful