FAQ Search

Is 30 mA earth leakage protection available for the Powerpact H and J frame circuit breaker?

Yes, the ELM150HD for the H frame breaker and ELM250JD for the J frame breaker provide 30 mA to 3 A sensitivity. The circuit breaker must have a 48Vdc shunt trip. Suffix SP for factory installed or S29392 field installable.


CTA-ID : 2051768
FA129021  |  14-Jan-2011  | Selection
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful