What is the correct neutral assembly for a P1200R, P1200S or P1200AWK circuit breaker enclosure? Several different numbers are given in prior catalogs, such as SN1200NA, H1200SNE4, or the SN1200.
Prior docments have been printed with incorrect information. If the P frame Power Pact breaker being used IS NOT provided with integral ground fault, use neutral assembly SN1200. If the P frame Power Pact breaker being used IS provided with integral ground fault, use neutral assembly S33576MK and order the Neutral CT S33576 separately.
CTA-ID : 2050188
CTA-ID : 2050188
Answers which others found helpful |