Is the neutral CT included with the GFM150HD or GFM250JD?
No, It is not included. The neutral CT part number is GFM25CT
CTA-ID : 2037127
FA122286 |
14-Jan-2011
|
Selection
PDF
Email
Bookmark
Print
Answers which others found helpful
> Can a HDL, HGL, HJL or HLL circuit breaker and GFM150HD ground fault unit be installed into a J250F enclosure?
> Can a HDL, HGL, HJL or HLL circuit breaker and GFM150HD ground fault unit be installed into a J250DS enclosure?
> On the ground fault modules for the H and J Frame circuit breaker, does the push to test feature require an external 12VDC to power the shunt trip coil? Is an external source necessary to activate the test feature?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel