Do the RPF Zelio power relays mount directly to din rail?
Yes. No socket is required. Terminations are made with quick connects.
CTA-ID : 2036755
FA121994 |
14-Jan-2011
|
Product Features
PDF
Email
Bookmark
Print
Answers which others found helpful
> Is there a DIN rail mount for a REG48PUN2LJLU temperature sensor?
> Do RE11 Relays mount on Din Rail?
> What is the catalog number of the Zelio Logic relay provided with the SR2PACKBD?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel