Can you lock off the QO circuit breakers when installed in the PowerBus plug in units?
Yes, if a floor operator attachment, PBFO100QO, is installed.
CTA-ID : 2035663
FA121942 |
14-Jan-2011
|
Selection
PDF
Email
Bookmark
Print
Answers which others found helpful
> Does the PBFO100QO turn all the QO breakers on & off?
> Can 1, 2 and 3 pole QO and QOB breakers be used in the Powerbus 225 - ``Ready-To-Assemble`` Plug in Unit Enclosures?
> Can a QOB-VH breaker be installed in a PowerBus225 plug-in unit?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel