Explain how End Closing Plates are installed on the sides of EZ Meter-Pak Main Devices?
EZM main devices are supplied with two closing plates, one for each side of the enclosure to cover and seal openings for horizontal cross bus.
RIGHT SIDE Closing Plate (Cat. No.: EZMSCAP, 1 inch wide) is secured to box side by (3) 1/4-20 captive screws and (3) 1/4``-20 star washer hex nuts. Two sealing wing nuts for this side are provided in a bag assembly packed with each main device. Holes in wing nuts and lanced ears in the closing plate are provided to seal closing plate to box sides. Install one wing nut on screw extending through closing plate at bottom center and another wing nut on screw extending through closing plate at the top front to seal.
LEFT SIDE Closing Plate (Cat. No.: EZMCAP, 2 inches wide) secured to box side by (3) 1/4``-20 carriage head screws and (3) 1/4``-20 star washer hex nuts. Two sealing wing nuts for this side are provided in a bag assembly packed with each main device. Holes in wing nuts and lanced ears in the closing plate are provided to seal closing plate to box sides. Install one wing nut on screw extending through closing plate at bottom center and another wing nut on screw extending through closing plate at the top front to seal. When sealing is not required, install screws from outside to inside of unit and secure with hex nuts.
When adding onto an existing EZM (Series M01, M02 or M03) metering equipment line-up, repeat this procedure by moving End Closing Plate to end of line-up.
CTA-ID : 2033575
RIGHT SIDE Closing Plate (Cat. No.: EZMSCAP, 1 inch wide) is secured to box side by (3) 1/4-20 captive screws and (3) 1/4``-20 star washer hex nuts. Two sealing wing nuts for this side are provided in a bag assembly packed with each main device. Holes in wing nuts and lanced ears in the closing plate are provided to seal closing plate to box sides. Install one wing nut on screw extending through closing plate at bottom center and another wing nut on screw extending through closing plate at the top front to seal.
LEFT SIDE Closing Plate (Cat. No.: EZMCAP, 2 inches wide) secured to box side by (3) 1/4``-20 carriage head screws and (3) 1/4``-20 star washer hex nuts. Two sealing wing nuts for this side are provided in a bag assembly packed with each main device. Holes in wing nuts and lanced ears in the closing plate are provided to seal closing plate to box sides. Install one wing nut on screw extending through closing plate at bottom center and another wing nut on screw extending through closing plate at the top front to seal. When sealing is not required, install screws from outside to inside of unit and secure with hex nuts.
When adding onto an existing EZM (Series M01, M02 or M03) metering equipment line-up, repeat this procedure by moving End Closing Plate to end of line-up.
CTA-ID : 2033575
Answers which others found helpful |