FAQ Search

Is an external motor overload relay required when the Output Phase Fault is disabled on the Altivar ATV66?

Yes it is recommended to use an external motor overload relay.


CTA-ID : 6720
FA115531  |  14-Jan-2011  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful