Is there a lug for a MGP36800 breaker that will allow 4 -3/0 wires per phase?
AL1200P24K which is good for 4 wires 3/0 to 500 kcmil wires.
CTA-ID : 2026757
FA115530 |
14-Jan-2011
|
Selection
PDF
Email
Bookmark
Print
Answers which others found helpful
> Can I get a lug that would accommodate two 600 kcmil conductors on an MGP36800 breaker?
> What is number for the 800A 3 pole vertically mounted main breaker used in the HCM, HCP, and the HCW I-Line panelboard?
> What is the main breaker in an HCM18738MP?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel