Are the ATS48 soft starters available in NEMA 3R ratings?
Yes. Nema 3R is available in the enclosed soft starter product line.
See the attached document.
CTA-ID : 2016091
FA108859 |
23-Jul-2012
|
Product Features
PDF
Email
Bookmark
Print
Answers which others found helpful
> Is the enclosed ATS48 rated for service entrance?
> Do we offer the ATS48 in NEMA 7 ratings?
> What are the BTU ratings for ATS48`s from 50-500 HP, 230Vac and 460Vac units?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel