FAQ Search

Is there a NEMA 4X or Type 4X handle operator available for the D10S* disconnect switches?

No, the rotary handle operating mechanisms available are rated NEMA Type 1, 3, 3R, 4 and 12 only.


CTA-ID : 2015028
FA107923  |  14-Jan-2011  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful