FAQ Search

What is the part number for a Dynamic Braking Resistor kit for an ATV28HU90M2U?

The part number is VW3A66714 for HU90M2U - D12M2U
The part numbers for the entire ATV28 line can be located in the July 1998 VD0C06N908C dynamic brake bulletin on page 47 which has the catalogs numbers listed with corresponding drives.  

The ATV66, ATV58, ATV18 & ATV28 all use the same dynamic brake kits for their respective sizes.

Also located in pricing guide.


CTA-ID : 2011782
FA105320  |  18-Jun-2012  | Selection
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful