can we get 3-NO aux contacts on a GJL breaker?
NO. You can get only 1-NO & 1-NC (1a1b), plus an alarm switch
CTA-ID : 2009118
FA103637 |
18-Jun-2012
|
Product Features
PDF
Email
Bookmark
Print
Answers which others found helpful
> Can we get 2-n.o. aux contacts on a GJL breaker?
> What are the ratings for the AAC 1a1b aux switch contacts for the GJL Circuit Breaker?
> What is suffix 2307 on an FAL 3 pole breaker?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel