What is the part number for a Dynamic Braking Resistor kit for an ATV28HU29N4U?
The part number is VW3A66711 for HU18N4U - U72N4U
The part numbers for the entire ATV28 line can be located in the July 1998 VD0C06N908C dynamic brake bulletin on page 47 which has the catalogs numbers listed with corresponding ATV18 drives.
The ATV66, ATV58, ATV18 & ATV28 all use the same dynamic brake kits for their respective sizes.
CTA-ID : 2006258
The part numbers for the entire ATV28 line can be located in the July 1998 VD0C06N908C dynamic brake bulletin on page 47 which has the catalogs numbers listed with corresponding ATV18 drives.
The ATV66, ATV58, ATV18 & ATV28 all use the same dynamic brake kits for their respective sizes.
CTA-ID : 2006258
Answers which others found helpful |