What Class R Fuse Kit is used with the H466, Series E safety switch?
Use HRK4060. Two kits required per switch.
CTA-ID : 2003843
FA100341 |
14-Jan-2011
|
Selection
PDF
Email
Bookmark
Print
Answers which others found helpful
> What is the Electrical Interlock Kit for a H466 , Series E safety switch ?
> What are the repair parts for a H466 Series E2 and E4 Heavy Duty Safety Switch?
> What is the rating of the number of switching operations of Square D, 600A, Heavy Duty, E-Series Safety Switches? These ratings are also sometimes referred to as Endurance operations and Horsepower-overload operations.
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel