FAQ Search

Is there a Class 9422 operating mechanism for the Powerpact H and J Frame breakers?

The following are available and can be located within the e-catalog at 7-21 and 7-22 or via the attached links.

Cable operators; 9422CSF30, 9422CSF50, 9422CSF70 & 9422CSF10.
Shaft driven; 9422RQ1.
NOTE: 9422A1 or 9422A2 Style flange handle must be purchased separately.



CTA-ID : 2027583
FA116985  |  29-Jul-2012  | Selection
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful