Can you get a run status indication from my ATV28 drive?
Yes. You can go to the I/O - menu and if want to have logic input to be high when above 0hz which is a valid reference when have direction signal may want to set R2 to Frequency threshold attained ( FtA ).
When set logic output to this it is in a state of 1 (on or closed) if the motor frequency is greater than or equal to the frequency threshold set by the Ftd parameter in the SEt - menu
(You can set FTD to a value of 1 and therefore it will not indicate running unless have frequency greater than 0hz.)
CTA-ID : 2009992
When set logic output to this it is in a state of 1 (on or closed) if the motor frequency is greater than or equal to the frequency threshold set by the Ftd parameter in the SEt - menu
(You can set FTD to a value of 1 and therefore it will not indicate running unless have frequency greater than 0hz.)
CTA-ID : 2009992
Answers which others found helpful |