What is the measurement accuracy of the Micrologic 5.0P, 6.0P, 5.0H and 6.0H trip units (including the sensors)?
Voltage (V) 1%
Current (A) 1.5%, higher accuracy (1%) can be achieved with special calibration on the current transformer (CT characterization option).
Frequency (Hz) 0.1 Hz
Power (W) and energy (Wh) 2.5%
CTA-ID : 8803
Current (A) 1.5%, higher accuracy (1%) can be achieved with special calibration on the current transformer (CT characterization option).
Frequency (Hz) 0.1 Hz
Power (W) and energy (Wh) 2.5%
CTA-ID : 8803