FAQ Search

Is the H60XFA Enclosed Molded Case Switch suitable for use in Division 1 and Division 2 Hazardous Locations?

Yes, the H60XFA is suitable for use in Hazardous Locations defined by the National Electrical Code (NEC) as Class I, Groups C & D, Divisions 1 & 2; Class II, Groups E, F & G, Divisions 1 & 2; or Class III, Divisions 1 & 2. The device will be marked for Class and Group, but is not required to be marked for Division per NEC 2005 Article 500.8(B)(2) FPN (Fine Print Note).
This device is UL Listed and CSA Certified.


CTA-ID : 9313
FA93077  |  14-Jan-2011  | Codes/Std/Certification
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful