Can the DRR relay contacts operate 120vac on the Omegapak 8804 Type PT/VT with the option card installed?
Yes. The relay is rated 5 amps at 24vdc 120 vac.
CTA-ID : 4176
FA91258 |
14-Jan-2011
|
Product Features
PDF
Email
Bookmark
Print
Answers which others found helpful
> What do modification numbers E08 and A08 represent for the Omegapak 8804?
> What is the service bulletin part number of the Types MC30 ( PT-Mod H08; VT-Mod H07; part number 52011-548-53 {drive run relay}), MC31 (PT-Mod G08; VT-Mod G07; part number 52011-548-52 {non-isolated input}), MC32 (PT-Mod F08; VT-Mod F0 for the Omegapak 8804?
> Are the 8803 drives repairable?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel