What is the number for a EHB 3 pole 125a breaker.
There is no EHB 125 amp breaker.
CTA-ID : 1342
FA91108 |
14-Jan-2011
|
Selection
PDF
Email
Bookmark
Print
Answers which others found helpful
> What is the catalog number for the device that takes two pole spaces to mount in a QO load center and is similar to a circuit breaker except that it has lugs only to give a feed thru option?
> Is there a restriction as to where a 125 amp 3 pole ED, EG, or EJ breaker can be mounted in a 250 amp max NF interior?
> Can I mount (2) three pole ED, EG, or EJ 125 amp breakers in a 250 amp maximum panel?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel