What is the part number for a signal isolation module that can be used on the 4-20mA speed reference coming from a PLC and inputting into the Altivar ATV66?
The part number is 52011-889-50.
CTA-ID : 7057
FA90056 |
14-Jan-2011
|
Selection
PDF
Email
Bookmark
Print
Answers which others found helpful
> What is the part number for the signal converter used on Econoflex with Modification J09 to allow 0-10 VDC speed input instead of the standard 4-20 mA source?
> Can you run two Altivar ATV66 drives with the same start stop and analog 10V signal for the speed reference?
> How is the Altivar ATV66 drive programmed to go to a preset speed if the speed reference follower signal is lost to AI2 analog input?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel