What is the part number for the 8803 Omegapak constant torque drive`s main control board?
The correct part number is VX4A455SD. The same control board was used independent of any power ratings.
CTA-ID : 1928
FA88053 |
14-Jan-2013
|
Selection
PDF
Email
Bookmark
Print
Answers which others found helpful
> What is CLI, current limit, adjustable range on the Altivar ATV58?
> What is the part number for the ATV45 drive`s main control board ?
> What would cause an Altivar 66 drive`s keypad to malfuction and display a Keypad Link Fault when the VW3A66901T memory card is installed?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel