FAQ Search

Does the EV230WSR charging station use any energy when in the standby mode? In other words, when no vehicle is being charged?

Yes, a very minimal amount of energy is used when the charger is in standby mode. In normal ambient temperature (25 Deg C/77 Deg F) and normal voltage (240Vac) the charging station uses 1.85 Watts of energy. The wattage is calculated based on a current draw of 0.0163 Amps at 240Vac, Power Factor of 0.47.


CTA-ID : 2059998
FA144684  |  07-May-2012  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful