FAQ Search

What are the repair parts for a HU265AWK Series E2 Heavy Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Complete interior - HUN265AE2 (includes line base assembly, arc suppressor assembly, Box insulator, line phase insulators and mounting hardware)
Line base assembly - 40552-212-50 SEL (2-required and arc suppressor assembly is not included)
Arc suppressor assembly - 40512-708-50 SEL (2-required) (OBSOLETE replaced by 4051270850)
Small lug assembly - 40560-270-50 (COPPER LUG/OBSOLETE)
Small lug Replacement- 40251-136-50 (Aluminum Lug Replacement/will accept Al/Cu Conductors)
Large lug assembly - 40256-026-50 (requires one per base assembly)
Line base phase insulator - 40552-193-01 (1 required)
Line base mounting screws - 40206-009-01 (2 required per base assembly)
Handle assembly - 40512-172-50 SEL
Vault handle - 40512-194-50 SEL
Handle knob kit - 40283-435-50 (the black & red knob at the end of the handle)


CTA-ID : 2054930
FA131008  |  14-Jan-2011  | Maintenance
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful