FAQ Search

To add a CE3100B to an existing NHDP panel?

The CE3100B breaker is obsolete, as are the CE3100E CE3100N and CE3100H Breakers.
There are no replacement breakers or hardware available to mount alternative breakers in the NHDP panels.

Suggested alternative panel is the Square D NF panel.


CTA-ID : 2053883
FA130169  |  14-Jan-2011  | Cross Reference
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful