To add a CE1015E 15A 1 pole breaker to an existing NHDP panel?
The CE1015E breaker is obsolete.
Alternative breaker is an FFGP16015 with FF22NHDP mounting kit and MHMHDP mounting screws. Both breakers are rated at 18KAIC at 600V. Up to 6 FFGP breakers can mount on this hardware kit.
This will mount in 22 inch wide NHDP panels only. They will not mount in the older 20 inch wide NHDP panels.
CTA-ID : 2053897
Alternative breaker is an FFGP16015 with FF22NHDP mounting kit and MHMHDP mounting screws. Both breakers are rated at 18KAIC at 600V. Up to 6 FFGP breakers can mount on this hardware kit.
This will mount in 22 inch wide NHDP panels only. They will not mount in the older 20 inch wide NHDP panels.
CTA-ID : 2053897
Answers which others found helpful |