FAQ Search

To add a CE1015N 15A 1 pole breaker to an existing CDP panel?

The CE1015N breaker is obsolete.
Alternative breaker is an FFJP16015 with FFCMH mounting kit. Both breakers are rated at 25KAIC at 600V. Up to 6 FFGP breakers can mount on this hardware kit. Only FF type breakers can mount on this hardware and it takes both sides of the panel.



CTA-ID : 2053895
FA130070  |  14-Jan-2011  | Cross Reference
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful