FAQ Search

Is there a Generator Interlock Kit for a HOMELINE 100 or 125 Ampere QOM1 main breaker loadcenter, that can be interlocked with a 2 pole branch breaker?

Yes, but only for Series S1 (Nema 1) and Series S1 or S2 (Nema 3R) load centers. Use HOMCRBGK1. This kit will interlock the QOM1 main breaker in a 100A or 125A HOMELINE loadcenter with a HOM 2P branch breaker (15 - 125A).


CTA-ID : 2052557
FA129463  |  14-Jan-2011  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful