S29340: What is the UL file for this handle (door mounted rotary handle for Powerpact H/J breakers?
It is E103955.
CTA-ID : 2051709
FA129032 |
14-Jan-2011
|
Codes/Std/Certification
PDF
Email
Bookmark
Print
Answers which others found helpful
> What is the part number for the door mounted rotary operating handle for a Powerpact H and J frame breaker?
> Door mounted rotary handle S29338 for Powerpact H and J frame breaker: Do we have a way to lock in the on position?
> Is the shaft included with a S29338 door mounted rotary handle for the Powerpact H and J frame?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel