Can a HOM4252L200TC, Series S01 load center be top or bottom fed?
Yes. This load center can be mounted with the Main Lugs positioned at the top of the interior for a top feed application. The complete load center can also be rotated 180 degrees to position the Main Lugs at the bottom of the interior for a bottom feed application. No field modifications are required.
CTA-ID : 2051347
CTA-ID : 2051347
Answers which others found helpful |