Do you use a 2 or 3 pole main breaker in a single phase NQ panel?
You use a 2 pole main breaker if you are back feeding the main but if you are using a main breaker kit then you use a 3 pole main.
CTA-ID : 2050277
FA127959 |
14-Jan-2011
|
Application
PDF
Email
Bookmark
Print
Answers which others found helpful
> What type of hub is available for use on the EZM Main Circuit Breaker, Main Fusible Switch or Main Lugs Terminal Boxes?
> Are single phase main breaker I-Line panels constructed with two pole or three pole main breakers?
> Can an NQMB4LA main breaker adapter kit be used with either a two pole or three pole main breaker?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel