FAQ Search

What is the NEMA rating or IP degree of protection for the door-mounted S29338 RE10 and S29340 RE20 rotary handle operator for the Powerpact H and J breaker?

S29338 and S29340 are IEC-Style Door-Mounted Rotary Operating Handles. The handle mechanism can be used in NEMA 12 enclosure applications. Degree of protection: IP40 as per IEC 529.



CTA-ID : 2049037
FA127576  |  14-Jan-2011  | Codes/Std/Certification
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful