FAQ Search

On the ground fault modules for the H and J Frame circuit breaker, does the push to test feature require an external 12VDC to power the shunt trip coil? Is an external source necessary to activate the test feature?

The ground fault module is self powered to power the 12VDC shunt trip, but requires a 120V external source to operate the test feature.


CTA-ID : 2049011
FA127482  |  14-Jan-2011  | Selection
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful