FAQ Search

Can a shunt trip accessory be added to an EZM31600CB?

Yes. The main breaker used is the PAF2036. The PA11021 shunt trip accessory can be field installed into the circuit breaker. This shunt trip module is suitable for 120, 208 or 240 Vac. Other shunt trip modules available are PA11042 (24 Vac), PA11086 (208 or 480 Vac), PA11027 (24 Vdc), PA11028 (48 Vdc), PA11029 (125 Vdc) and PA11030 (250 Vdc).


CTA-ID : 2048870
FA127376  |  14-Jan-2011  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful