FAQ Search

What are the repair parts for a QMB223TW, Series E1 (E01)?

The QMB device is a twin switch, meaning it contains two switches in the one device. Parts are listed per switch. Only the parts listed below are considered field replaceable:
Arc Shield/Suppressor Assembly (1 required) - 4051239950
Load Base Assembly (1 required, includes lugs) - 4052068150
Load Base Mounting Screw (2 required per load base) - 4020506501
Handle Knob Kit - 4028343750




CTA-ID : 2048437
FA126551  |  14-Jan-2011  | Maintenance
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful