Search FAQs
Can a cover with a door be ordered separately for use with the QO612L100S?
Issue:
QO612L100S has no door with the cover.
Product line:
QO load centers
Cause:
Application
Resolution:
Yes it can, but it would require ordering a replacement cover with door and the labeling is NOT supplied with any of the replacement covers. Also, the cost of the replacement cover may exceed or be close to a complete new load center of this same size (like the QO612L100DS). One might consider purchasing a complete load center that comes with a door part of the cover and use the cover on with the existing load center if already installed.
The the cover with door catalog number for load center Series G1, G3, or G4 is: 4055345351.
QO612L100S has no door with the cover.
Product line:
QO load centers
Cause:
Application
Resolution:
Yes it can, but it would require ordering a replacement cover with door and the labeling is NOT supplied with any of the replacement covers. Also, the cost of the replacement cover may exceed or be close to a complete new load center of this same size (like the QO612L100DS). One might consider purchasing a complete load center that comes with a door part of the cover and use the cover on with the existing load center if already installed.
The the cover with door catalog number for load center Series G1, G3, or G4 is: 4055345351.