FAQ Search

What is the voltage and AIC rating on the Multi 9, C45 breakers

The 1 pole breaker is rated 5 kA @ 240V, and the 2, 3, 4 pole is rated 5 kA @ 415 V.


CTA-ID : 2041467
FA124454  |  14-Jan-2011  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful