FAQ Search

Can the VISI-TITE Bolt used in Old Style EZ Meter-Pak (Series: 1, 2 or 3) be replaced in the field?

No. Old Style EZM made use of a Sliding Joint-Pak and a single VISI-TITE Two-Headed Joint Bolt in each cabinet. Once the outer head of this VISI-TITE Bolt was broken off (at the first installation), a second hex head remains that can now be used as a normal bolt. A label near the bolt head indicates the proper torque to be applied the next time this sliding joint-pak needs to be re-installed.


CTA-ID : 2035112
FA121771  |  14-Jan-2011  | Maintenance
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful