FAQ Search

What is the catalog number for the solid neutral that can be used with a MA1000R enclosure?

AL800SN is the solid neutral that can be used with a MA1000R enclosure.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.


CTA-ID : 2034915
FA121676  |  14-Jan-2011  | Selection
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful