FAQ Search

Can we offer 100% Rated Main Circuit Breakers or Main Fusible Switches for use with EZ Meter-Pak metering equipment?

We are not able to offer integral mounted 100% Rated EZM Main Circuit Breakers or 100% Rated EZM Main Fusible Switches.
We can however feed an EZM Main Lugs Tap Boxes from remote mounted locations with some 100% Rated Square D Circuit Breakers.
NOTE: Meter Center Fault Current Levels when fed from upstream mounted 100% Rated Square D Circuit Breakers may have some restrictions.
Refer to Digest 174, Page 2-9 for UL Listed Meter Center Short Circuit Current Ratings (SCCR).
Meter Center Horizontal Cross Bus must not be exceeded. Square D offers mains and branch units with 800A continuous and 1200A continuous
ratings. Branch units having 800A cross bus can be upgraded to 1200A.


CTA-ID : 2035653
FA121427  |  14-Jan-2011  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful