FAQ Search

On a CU816D400CN, what is the difference between the Series M02 and M03 designs?

The difference is the meter socket used. The Series M02 design used a meter socket that was purchased from Cooper B-Line (part number 21324CD). The Series M03 design is using a meter socket that is manufactured by Square D Company (part number 73294-902-50). The meter sockets are not compatible between the two different designs.


CTA-ID : 2034472
FA121315  |  14-Jan-2011  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful