Can a 5.0P or 5.0H trip unit be used for ground fault alarm without tripping?
Yes. To have ground-fault alarm without tripping, add a programmable contact module (M2C or M6C), and program the trip unit for alarm.
Neither the 5.0 nor 5.0A trip units can be used because those trip units do not have the required programming functionality. If replacing a standard trip unit (not A, P or H), the 12-pin connector for the trip unit (kit S33101 for Masterpact, S33100 for Powerpact) must also be ordered.
CTA-ID : 2031878
Neither the 5.0 nor 5.0A trip units can be used because those trip units do not have the required programming functionality. If replacing a standard trip unit (not A, P or H), the 12-pin connector for the trip unit (kit S33101 for Masterpact, S33100 for Powerpact) must also be ordered.
CTA-ID : 2031878