What is the UL file number on a HOMCGK2 and HOMRBGK2 generator kit?
UL file is E6294, Volume 7, Section 16, Page 1. There is a label in the box that needs to be attached to panel as well.
CTA-ID : 2031278
FA118962 |
14-Jan-2011
|
Product Features
PDF
Email
Bookmark
Print
Answers which others found helpful
> Can a HOMRBGK2 Generator Interlock Kit be used with a HOM816M150FTRB?
> Can a HOMRBGK2 Generator Interlock Kit be used with a HOM816M200FTRB?
> If a HOMCGK2C, generator interlock kit, is Installed on a bottom fed main breaker in his Homeline load center, and the Label is oriented upside down, is there another label available that can be used, so it can be read correctly?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel