Are the option cards and serial communications cards for the ATV58 CSA approved?
Yes the ATV58 and all of its options (VW3A58****) are CSA approved.
CTA-ID : 2015351
FA118524 |
18-Jun-2012
|
Codes/Std/Certification
PDF
Email
Bookmark
Print
Answers which others found helpful
> Is the part number VW3A58352U for Lonworks option card available for the ATV58?
> Does the LUFP9 Devicenet option used with the drive require external 24v power supply?
> Can the ATV58 115VAC I-O Option kit part number VW3A58275U be installed on a drive that also has a serial communications card installed?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel