FAQ Search

Is the enclosure box or cover available for the Class 2510 Type MBW__ or Type MCW__ NEMA 4 stainless steel or NEMA 4X glass-polyester enclosed manual starter?

No, the complete enclosure which includes box and cover complete with external start/stop operator must be replaced. This applies regardless of the Series (A,B or C). Replacement enclosure is part number for stainless steel is 9991MW11, 9991MW1 for glass-polyester.


CTA-ID : 2026823
FA115723  |  14-Jan-2011  | Maintenance
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful