What is the part number for the door mounted rotary operating handle for a Powerpact H and J frame breaker?
Catalog number for black is S29338; catalog number for red is S29340
CTA-ID : 2025215
FA114139 |
14-Jan-2011
|
Selection
PDF
Email
Bookmark
Print
Answers which others found helpful
> What is the catalog number suffix for a factory installed direct mounted rotary operated handle for PowerPact H- and J- frame breakers?
> What is the part number for a field installable direct mounted rotary operated handle for PowerPact H- and J- frame breakers?
> What is the NEMA rating or IP degree of protection for the door-mounted S29338 RE10 and S29340 RE20 rotary handle operator for the Powerpact H and J breaker?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel