What is the control coil operating voltage range for the Class 8903 Type L or Type LX Lighting Contactor?
85% to 110% of marked or rated voltage.
CTA-ID : 2024199
FA113400 |
14-Jan-2011
|
Product Features
PDF
Email
Bookmark
Print
Answers which others found helpful
> What power poles can be field added to the Class 8903 Type L*1000 or 8903LX*1000 lighting contactor?
> What power poles can be field added to the Class 8903 Type L*80 or 8903LX*80 lighting contactor?
> What are the UL coordinated short circuit or AIC ratings for the Class 8903 Type L and Type LX lightng contactors?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel