FAQ Search

Is it possible to defeat, turn off, or otherwise remove the ground-fault feature from an SE type circuit breaker with a Micrologic Series B trip unit?

The trip unit on the SE breaker can be replaced with an LSA (GF Alarm) trip unit. Ground fault can be disabled using jumpers described in the instruction manual for primary injection testing only. The ground fault function can be minimized by setting the pickup and delay to maximum.


CTA-ID : 2020620
FA111099  |  14-Jan-2011  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful