FAQ Search

What is the part number for the Cooling Fan for the ATS46C17N , ATS46C21N , ATS46C25N , ATS46C32N , ATS46C41N , ATS46C48N , ATS46C59N , ATS46C66N , ATS46C79N , ATS46M10N or ATS46M12N.

The replacement part number is VZ3V001.
NOTE: The ATS46C79N, ATS46M10N or ATS46M12N use two of these fan kits per soft starter.
This fan is the one that is actually mounted in the soft starter.
If the fan that is needed is part of an enclosure, this would not be the correct part number.


CTA-ID : 2010179
FA110980  |  14-Jan-2011  | Selection
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful